Essentials Cables

High-performance servo systems require high signal integrity. Electrical noise in the system can cause degraded performance or even instability. Therefore, well-designed connectors and cables are as critical to the system as are motors, drives and controls. A system is only as good as its weakest link.

Kollmorgen can only guarantee the performance and quality of its servo systems when you use servo motors, servo drives and cables supplied by Kollmorgen. Not all cables are created equal.

The Kollmorgen Essentials Cable not only works with Kollmorgen Essentials Motors, but will also work with Kollmorgen AKM and AKM2G servo motors configured with a “9” connector option for AKM or “A” connector option for AKM2G and SFD-M or SFD-3 feedback.