Holding Brake Functionality

The brake function must be enabled through a drive parameter.

  • The following image shows the timing and functional relationships between the controlled stop signal, speed, and braking force.
    • All values can be adjusted with drive parameters; values in the diagram are default values.
  • The parameters shown are specific to Kollmorgen AKD2G drives and Kollmorgen Essentials Drive.
  • The drive speed setpoint is internally driven down an adjustable ramp (AXIS#.CS.DEC) to 0 V.
  • With default values, the output for the brake is switched on when the speed has reached 5 rpm (AXIS#.ZEROV) for at least 6 ms (AXIS#.ZEROT).
  • The rise (tBRH[ms]) and fall (tBRL[ms]) times of the holding brake built into the servo motor are different for the various types of servo motor.