Technical Data Terminology

  • See the individual servo motor series sections for their respective technical data, dimensional drawings, and key and keyway dimension details.
  • All data is valid for 40 °C environmental temperature and 100K overtemperature of the winding.
  • Determination of nominal data with constant temperature of adapter flange of 65 °C.
  • The data can have a tolerance of +/- 10%.

Term

Definition

Peak Current, 
(pulse current) 
I0max [A]

  • The Peak Current (effective sinusoidal value) is several times the rated current, depending on the servo motor winding.
  • The actual value is determined by the peak current of the drive which is used.

Rated Torque, Mn [Nm]

  • The Rated Torque is produced when the servo motor is drawing the rated current at the rated speed.
  • The Rated Torque can be produced indefinitely at the rated speed in continuous operation (S1).

Release Delay Time tBRH[ms] / Engage Delay Time tBRL[ms] of the brake

These constants define the response times of the holding brake when operated with the rated voltage from the servo drive.

Rotor Moment of Inertia, J [kg-cm²]

The constant J is a measure of the acceleration capability of the servo motor.

Example: At I0, the acceleration time tb from 0 to 3000RPM is given as:

with M0 in Nm and J in kg.cm².

Standstill Current, I0rms [A]

The standstill current is the effective sinusoidal current which the servo motor draws at 0<n<100RPM to produce the standstill torque.

Standstill Torque, M0 [Nm]

The standstill torque can be maintained indefinitely at a speed 0<n<100RPM and rated ambient conditions.

Thermal Time Constant, tth [min]

  • The constant tth defines the time for the cold servo motor, under a load of I0rms, to heat up to a temperature rise of 0.63 x 105 Kelvin.
  • This temperature rise happens in a much shorter time when the servo motor is loaded with the peak current.

Torque Constant, 

  • The Torque Constant defines how much torque in Nm is produced by the servo motor with 1A r.m.s. current.
  • The relationship is M=I x KT .

UN

Rated mains voltage.

Un

  • DC-Bus link voltage.

Voltage Constant, KErms [mV/min-1]

  • The Voltage Constant defines the induced servo motor EMF, as an effective sinusoidal value between two terminals, per 1000RPM.
  • Measured at 25 °C.