Fieldbus - EtherCAT
|
Name |
Description |
|---|---|
|
Reads a drive parameter by sending an ASCII command to a drive. |
|
|
Reads a single drive parameter by sending an ASCII command to a drive. |
|
|
Writes a drive parameter by sending an ASCII command to a drive. |
|
|
Returns a list of bad EtherCAT connections. |
|
|
Performs an action on an EtherCAT device. |
|
|
Provides the EtherCAT state and the port link status information for the EtherCAT device. |
|
|
Returns the EtherCAT device-specific information. |
|
|
Deprecated. |
|
|
Reads the EtherCAT master state and the lost frame counter to determine if EtherCAT is running normally. |
|
|
Reads cyclic parameter (byte offset format). |
|
|
Copies the Input (Tx) PDO object data from an EtherCAT cyclic frame to a byte array. |
|
|
Reads a 32-bit word from I/O nodes using a CANopen SDO read command. |
|
|
Reads data from an EtherCAT device using CANopen SDO read command. |
|
|
Returns the current number of working counter errors for the Sync unit. |
|
|
Writes cyclic parameter (byte offset format). |
|
|
Writes data to an Output Rx PDO object of the EtherCAT device in the cyclic EtherCAT frame. |
|
|
Writes a 32-bit word to I/O nodes using a CANopen SDO write command. |
|
|
Writes data to an EtherCAT device using a CANopen SDO write command.. |
|
|
Transfers safety parameters from the safety master to safety slave devices to initialize the safety network. |
Remarks
- The client (aka EtherCAT master) is the KAS Runtime application.
- The servers (aka EtherCAT slaves) are the drives and I/O nodes where data can be retrieved.
- The SDO function blocks only support the reading and writing of 32-bit values.
- It is the fundamental size of CANopen SDO calls.
Why use ECATReadSdo and ECATWriteSdo FBs?
- The ECATReadSdo and ECATWriteSdo response time is faster.
- The ECATReadSdoData and ECATWriteSdoData are used when the data size is greater than 4 bytes.
- They are preferred over DriveParamRead and DriveParamWrite.
Why use the DriveParam FBs?
Reasons to prefer the DriveParam FBs are:
- They allow direct use of the parameter name.
- Example: IL.LIMITP instead of the SDO index: 356Eh
- They can be used to setup a drive terminal in the HMI application.
- This is similar to the Terminal view available in the AKD widget embedded in the KAS-IDE.