MC_GrpReadStatus

PLCopen motion icon Pipe Network motion icon

 Function Block - Returns the status of an axes group.

  • See Coordinated Motion, the top-level topic for Coordinated Motion.
  • MC_GrpReadStatus returns the status of an axes group.
    • This function block does not cause any motion.
  • See Group State Diagrams.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Enable

BOOL

FALSE, TRUE

N/A

No default

If TRUE, the axes group status is read.

AxesGroup

AXES_GROUP_REF

No range

N/A

No default

The axes group the status is read from.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Valid

BOOL

FALSE, TRUE

N/A

TRUE of valid outputs are available.

GroupMoving1

BOOL

FALSE, TRUE

N/A

  • The axes group is in the Moving state.
  • This indicates the group is enabled and currently executing a coordinated motion command.

GroupHoming1

BOOL

FALSE, TRUE

N/A

Not supported.

GroupErrorStop1

BOOL

FALSE, TRUE

N/A

The axes group is in the ErrorStop state due to an axis error or group error.

  • The group cannot accept coordinated motion commands.
  • The execution of MC_GrpReset is required to change the group’s state from ErrorStop to Standby.

GroupStandby1

BOOL

FALSE, TRUE

N/A

The axes group is in the Standby state.

  • The group:
    • Is enabled and all its axes are enabled.
    • Is not currently executing a coordinated motion command.
  • The axes group is ready to accept coordinated motion commands.

GroupStopping1

BOOL

FALSE, TRUE

N/A

The axes group is in the Stopping state due the execution of MC_GrpStop.

  • The axes group is enabled but cannot accept coordinated motion commands while in the Stopping state.
  • The axes group:
    • Remains in the Stopping state while MC_GrpStop is executing.
    • Will remain in the Stopping state while MC_GrpStop’s Execute input is held high.

GroupDisabled1

BOOL

FALSE, TRUE

N/A

The axis group is in the Disabled state and cannot accept coordinated motion commands.

ConstantVelocity

BOOL

FALSE, TRUE

N/A

TRUE if the commanded path velocity is the same between the current scan of the application program and the previous scan.

  • ConstantVelocity is always TRUE for Direct moves.
  • The commanded path velocity of Direct moves is always 0 (zero).

Accelerating

BOOL

FALSE, TRUE

N/A

TRUE if the commanded path velocity is accelerating between the current scan of the application program and the previous scan.

Decelerating

BOOL

FALSE, TRUE

N/A

TRUE if the commanded path velocity is decelerating between the current scan of the application program and the previous scan.

InPosition

BOOL

FALSE, TRUE

N/A

TRUE indicates that the axes group is “in position”.

These must be TRUE for the axes group to be in position:

  • The axes group is enabled.
  • There are no moves in the group’s queue.
  • The servo loop is closed for each axis in the group.
  • There are no moves in the individual axis queue for each axis in the group.
  • The command delta is zero for each axis in the group.
  • The actual position is within the In-Position Bandwidth of the command position for each axis in the group.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

INT

Enumerated

N/A

1 These outputs are mutually exclusive.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Check boolean status bits for an Axis Group
Inst_MC_GrpReadStatus( EnableGrpReadStatus, Group1_Ref );

IsGroupMoving:= Inst_MC_GrpReadStatus.GroupMoving;
IsGroupErrorStop:= Inst_MC_GrpReadStatus.GroupErrorStop;
IsGroupStandby:= Inst_MC_GrpReadStatus.GroupStandby;
IsGroupDisabled:= Inst_MC_GrpReadStatus.GroupDisabled;
Accelerating:= Inst_MC_GrpReadStatus.Accelerating;
IsConstantVelocity:= Inst_MC_GrpReadStatus.ConstantVelocity;
IsInPosition:= Inst_MC_GrpReadStatus.InPosition;

See Also

MC_ErrorDescription