MC_GrpSetOverride
Function Block - Sets the velocity factor that is multiplied to the commanded velocity of all axes in the group.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- This function or function block does not generate any motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- Changing the velocity factor during an S-Curve Corner transition does not change the profile of the transition.
- The new velocity factor is applied after the S-Curve Corner transition completes.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, changes the velocity multiplier for the axes group. |
|
AxesGroup |
No range |
N/A |
No default |
The axes group the velocity multiplier is applied to. |
|
|
VelFactor |
REAL |
0.0 to 2.0 |
N/A |
No default |
The new multiplier factor for the commanded velocity of the axes group. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Enabled |
BOOL |
FALSE, TRUE |
N/A |
Indicates that the override was successful. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the function block is executing. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
Enumerated |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Inst_MC_GrpSetOverride( EnableOverride, Group1_Ref, VelocityFactor );
See Also