MC_InitAxisFeedback

PLCopen motion icon

 Function - Initializes a PLCopen digitizing Axis' position data.

  • A call to this function is automatically generated when the application is compiled.
  • This call is based on the data entered in the PLCopen Axis Data dialog box.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

En

BOOL

FALSE, TRUE

N/A

No default

  • Request to Initialize a PLCopen Digitizing Axis.
  • This input is only applicable to FFLD programs.

AxisNumber

UINT[ ]

 

UINT

1 to 256

N/A

No default

Digitizing Axis number.

FeedbackPDOIndex

UINT

0 to 65536

N/A

No default

The object Index through which the feedback data is sent.

FeedbackPDOSubIndex

UINT

0 to 255

N/A

No default

The sub index of the object through which the feedback data is sent to the controller.

FeedbackDataResolution

UINT

1 to 32

N/A

No default

The resolution of the Encoder.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

ErrorID

DINT

No range

N/A

Indicates if the call failed or succeeded.

If the call succeeds, this is set to 0 (zero).

FBD Language Example

FFLD Language Example

Not available.

IL Language Example

Not available.

ST Language Example

(* MC_InitAxisFeedback ST example *)
// Initialize the digitizing Axis (Axis #3) with the Feedback object 0x60E4 subIndex 2.
Encoder resolution is 25bits.
ErrID := MC_InitAxisFeedback(3, 16#60E4, 16#02, 25);