MC_TouchProbe
Function Block - Arms a Fast Input and returns the latched position when the Fast Input event occurs.
-
-
- This function block starts a motion-related action and stores data for calculations and error checking.
- If using a dual-core controller, see Program a Multi-Core Controller.
- This function or function block does not generate any motion.
- See Function Blocks - General Rules about how inputs and outputs work.
- This function block captures an axis position
- When the Execute input transitions from low to high, the control requests the drive to arm its Fast Input to latch the axis position when a Fast Input occurs.
- The Axis input specifies which axis's position to latch and the TriggerInput input specifies which Fast Input to use and whether to trigger on the rising or falling edge of the Fast Input.
- When the Fast Input event occurs, the drive latches the axis's position.
- This function block then returns the latched position at the RecordedPosition output and set the Done output high.
- This process can be canceled with the AbortTrigger function block.
- If the WindowOnly input is high, the FirstPosition input and the LastPosition input define a window in which a Fast Input is accepted.
- Any Fast Input events that occur outside the window is ignored.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
On the rising edge, request to arm the input to return the latched position. |
|
Axis |
AXIS_REF |
1 to 256 |
N/A |
N/A |
Selects the axis the position is latched to. |
|
TriggerInput |
TRIGGER_REF |
See Description. |
N/A |
No default |
|
|
BOOL |
FALSE, TRUE |
N/A |
No default |
Enables a position latching window.
|
|
|
FirstPosition |
LREAL |
No range |
User units |
No default |
See the WindowOnly Description about how this input and the LastPosition input define the window.
|
|
LastPosition |
LREAL |
No range |
User units |
No default |
See the WindowOnly Description about how this input and the FirstPosition input define the window.
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
|
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
Indicates the specified input is:
|
|
CommandAborted |
BOOL |
FALSE, TRUE |
N/A |
|
|
Error |
BOOL |
FALSE, TRUE |
N/A |
|
|
ErrorID |
INT |
|
|
|
|
RecordedPosition |
LREAL |
|
User units |
|
Remarks
-
- There are differences in how MC_TouchProbe interacts with AKD and AKD2G drives.
See these topics for drive-specific information:
-
-
- The accuracy of captured position data depends on the travel velocity.
- See this article MC_TouchProbe and Time-Based Capture about how to correct for timing.
Example 1
If First Position ≤ LastPosition, the window in which a Fast Input is accepted is:
FastInputPosition ≥ FirstPosition AND FastInputPosition ≤ LastPosition
![]()
Example 2
If First Position > LastPosition, the window in which a Fast Input is accepted is:
FastInputPosition ≥ FirstPosition OR FastInputPosition ≤ LastPosition
![]()
Elements
This is the drive capture engine to be used.
INT TriggerInput.InputID
Valid values of InputID are:
- 0 = Touch Probe 1 / Capture Engine 0
- 1 = Touch Probe 2 / Capture Engine 1
This is the input signal’s edge to capture.
INT TriggerInput.Direction
Range = 1 to 2
- 1 = Rising edge.
- 2 = Falling edge.
-
- Trigger Direction is also sent to the servo drive and is shown in the WorkBench Position Capture screen Edge setup.
This is where the input comes from.
INT TriggerInput.TrigID
Range = 0 to 256.
0 = Trigger axis is to be the same as Axis.AXIS_NUM.
This is the capture method.
INT TriggerInput.TrigMode
Range = 0 to 1
- 0 = Time based capture.
- 1 = Position based capture.
- For position based capture, the TrigID must be the same as the AXIS_REF.
-
- The Mode (either Time or Position) must be configured the same in the servo drive.
This can be done either in:- COE Init commands and executed when the EtherCAT network is initialized (0x3460, subindex 3 and 4).
- The WorkBench Positon Capture screen.
Usage
This function block can be used to:
- Perform registration.
- Determine the position of a product.
- Measure product length.
Limitations
- Both high speed inputs cannot be used at the same time.
- The TrigMode option is only used by MC_TouchProbe.
Fast Homing - Inputs
See these topics:
- Example: Fast Homing with the Pipe Network Motion Engine Axis Pipe Block
- Example: Fast Homing with the PLCopen Motion Engine
- Fast Inputs with Pipe Network Motion
- Pipe Network Registration and Fast Homing
- Example: Registration Position Capture with Pipe Network Trigger Block
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_TouchProbe ST example *) |
See Also