MC_CamStartPos

PLCopen motion icon

 Function Block - Returns the slave axis position for starting an MC_CamIn move.

  • This function block returns the slave axis position for the specified profile, based on the current position of the master axis.
    • This slave axis position can be used to command the slave axis to move to the proper location prior to commanding a MC_CamIn move with StartMode = 0 (Start mode).
  • The typical application of MC_CamStartPos is to aid in positioning a slave axis to its starting position for a MC_CamIn move with a slave absolute profile.
  • See Position an Axis Before Starting Camming for instructions.

    • This function block starts a motion-related action and stores data for calculations and error checking.
    • If using a dual-core controller, see Program a Multi-Core Controller.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

Enable

BOOL

FALSE, TRUE

N/A

No default

Enables execution.

Master

AXIS_REF

AXIS_NUM - 1 to 256

N/A

No default

Master axis.

Slave

AXIS_REF

AXIS_NUM - 1 to 256

N/A

No default

Slave axis.

MasterOffset

LREAL

No range

User units

No default

  • Profile shift along the master axis.
  • This input is not used if the StartMode input is set to 1 for Resume Mode.

SlaveOffset

LREAL

No range

User units

No default

  • Profile shift along the slave axis.
  • This input is not used if the StartMode input is set to 1 for Resume Mode.

MasterScaling

LREAL

No range

User units

No default

  • Master axis scale factor.
  • Scaling must be a positive value greater than 0 (zero).

SlaveScaling

LREAL

No range

User units

No default

  • Slave axis scale factor.
  • Scaling must be a positive value greater than 0 (zero).

CamTableID

INT

0 to 255

N/A

No default

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

  • TRUE = the function block has successfully calculated the slave position.
  • The slave position is available at the SlavePos output.

Error

BOOL

FALSE, TRUE

N/A

  • TRUE = an invalid input was specified or an error occurred in the calculations.
  • The value at the SlavePos output is undefined.

ErrorID

INT

No range

N/A

SlavePos

LREAL

No range

User units

If the Done output is TRUE, this output returns the:

  • Position for the slave axis given the profile.
  • Current master axis position.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Inst_MC_CamStartPos( TRUE, Axis1, Axis2, MasterOffset, SlaveOffset, MasterScale, SlaveScale, Profile1CamTableID);