MC_StopRegist

PLCopen motion icon

 Function Block - Turns off registration for the specified axis and disarms the specified fast input.


  • To use Capture Engine 1, modify the input PDOs that are used and add the Latch Position 1 parameter.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

En

BOOL

FALSE, TRUE

N/A

No default

Enables execution.

Axis

AXIS_REF

1 to 256

N/A

N/A

Axis registration to turn off.

TriggerInput

TRIGGER_REF

See Description.

N/A

No default

Structure specifying the fast input. (to disarm)

The structure elements are:

DirectionINT

Range = 1, 5.

  • 1 = Rising edge.
  • 2 = Falling edge.
  • 3 = N/A
  • 4 = Toggle between both, falling edge first.
  • 5 = Toggle between both, rising edge first.

Valid values of InputID are:

  • 0 = Touch Probe 1 / Capture Engine 0
  • 1 = Touch Probe 2 / Capture Engine 1

TrigidINT

Range = 0 to 256.

  • Axis number of the fast input.
  • 0 (zero) indicates this trigger axis is to be the same as the Axis input. .

  • TrigMode INT (TriggerInput.TrigMode) is not presently supported by this function.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Execution successful.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

StopOK := MC_StopRegist( Axis1, Trig1);

See Also