MLAxisAddTq
Function - Set the additive torque value to the drive output (torque feed-forward).
- This function is only active after the MLAxisRatedTq function has been invoked.
- Using the PDOs for Kollmorgen Servo Drives, it also requires the IL.KBUSFF value to be set to 1 in the drive.
-
-
- This function or function block returns cached data.
- See Program a Multi-Core Controller.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
1 to 1024 |
N/A |
No default |
Pipe Network identifier of the axis block. |
|
Torque |
LREAL |
No range |
|
No default |
Requested additive torque value in N.m (Newton meter). |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisAddTq(PipeNetwork.Axis1, LREAL#10 ) ;
See Also