MLAxisAddress

Pipe Network motion icon

 Function - Returns the motion bus address of the axis.

  • Axes have the same address when they are mapped to the same multi-axis drive (e.g., the dual-axis AKD2G drive).
    • Example: If Axis1 is mapped to an AKD2G’s Drive Axis Number 1 and Axis2 is mapped to the AKD2G’s Drive Axis Number 2, both axes return the same address. (Figure 1)
    • Figure 1: Example of Axis 1 and Axis 2

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Returns TRUE when the function successfully executes.

Default (.Q)

DINT

No range

N/A

Returns the motion bus address of the axis.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Address := MLAxisAddress(PipeNetwork.AXIS1);