MLAxisGenEN

Pipe Network motion icon

 Function - Enables or disables the internal TMP generator of the axis.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Enable

BOOL

FALSE, TRUE

N/A

No default

Boolean switch to activate the generator.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 MLAxisGenEN( PipeNetwork.Axis1, true) ;

See Also

MLAxisGenIsEN