MLAxisGenWriteSpd

Pipe Network motion icon

 Function - Sets the speed of the internal generator of an axis.

This function or function block does not generate any motion.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Speed

LREAL

No range

User units / sec

No default

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 MLAxisGenWriteSpd(PipeNetwork.Axis1, 500 )  ;

See Also