MLAxisReadFBUnit

Pipe Network motion icon

 Function - Gets the feedback units per revolution value of the axis.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

FBUnitsPerRev

LREAL

> 0 (zero)

Feedback units / revolution

Returns the Axis Feedback Units per revolution.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Feedback_Units := MLAxisReadFBUnit(PipeNetwork.Axis1 )  ;