MLAxisReadModPos

Pipe Network motion icon

 Function - Gets the value period of the axis.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

ModuloPosition

LREAL

No range

User units

Returns the Axis Value Period.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Value_Period := MLAxisReadModPos(PipeNetwork.Axis1 )  ;