MLAxisReadVel

Pipe Network motion icon

 Function - Returns the actual velocity of the axis based on the data provided by the drive's feedback device.

In AKD, S300, and S700 drives:

  • The actual velocity is calculated internally by the drive.
  • The Velocity Actual Value object (CoE object 0x606C, subindex 0) must be included in the drive's Input (Tx) PDO data for the controller to read the axis actual velocity from the drives.
  • By default, the Velocity Actual Value object is included in the AKD PDOs 0x1B20, 0x1B22, and 0x1B23.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

Pipe network identifier of the axis block.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Velocity

LREAL

No range

User units / sec

The actual velocity of the axis.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Velocity := MLAxisReadVel(PipeNetwork.Axis1 ) ;

See Also