MLAxisWriteModPos

Pipe Network motion icon

 Function - Sets the value period of the axis.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

ModuloPosition

LREAL

No range

User units

No default

Sets the Axis Period Value when Mode is set to Modulo.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 
MLAxisWriteModPos(PipeNetwork.Axis1, 360) ) ;