MLPrfReadOOffset

Pipe Network motion icon

 Function - Returns the Output Offset value of a selected CAM Profile.

  • Offsets can be changed on the fly to modify the CAM Profile while maintaining its shape.
  • A change in output offset is equivalent to shifting the CAM Profile on the Y (or Output) Axis.

Figure 1: MLPrfReadOOffset

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ProfileID

DINT

1 to 1024

N/A

No default

ID number of an initialized CAM Profile.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Offset

LREAL

No range

User units

Returns the Output Offset of the selected CAM Profile.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Save value of output offset
CamOffset := MLPrfReadOOffset( Profiles.Profile_A );

See Also