MLPrfWriteOScale

Pipe Network motion icon

 Function - Sets the Output Ratio value of a selected CAM Profile.

  • Previous function name: MLPrfSetORatio
  • Ratios can be changed on the fly to modify the CAM Profile while maintaining its basic shape.
  • A change in output ratio is equivalent to stretching (flipping if negative - see MLPrfWriteOScale) the CAM Profile on the Y (or Output) Axis.

Figure 1: MLPrfWriteOScale

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

ProfileID

DINT

1 to 1024

N/A

No default

ID number of an initialized CAM Profile.

Ratio

LREAL

No range

N/A

No default

Desired new value of Output Ratio.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Change value of output ratio
MLPrfWriteOScale( Profiles.Profile_A , -180 );

See Also