Convertor
|
Name |
Description |
|---|---|
|
Connects the output of a pipe convertor block to an EtherCAT Output (Rx) PDO object. |
|
|
Connects a converter Pipe Block to the specified axis. |
|
|
Connects the output of a pipe to an axis data other than the control position. Connects an extra converter Pipe Block to the specified axis. |
|
|
Disconnect a converter Pipe Block from its associated axis. |
|
|
Initializes a converter Pipe Block. |
Purpose
The convertor block is necessary to define the connection between a pipe and a destination object.
- Depending on convertor mode, the incoming numerical values are converted to Position or Speed setpoints with no periodicity.
- This conversion has no effect on the axis units and their periodicity.
- This block must be present at the end of a pipe, typically right before an axis block. (Figure 1)
Figure 1: Example: Convertor - Position Mode - No Modulo
The Output position values are identical to input values when inputs in position mode (by range). (Figure 2 and Figure 3)
Parameters
|
Parameter |
Description |
|---|---|
|
Mode |
Determines the type of input to the Converter Object. The available modes are: Position
Speed
|
Associated Data
- OutputValue: Output value of the data flows.
- IslinkedToAxis: Boolean set to TRUE when the Convertor pipe block is linked to an axis block.