MLGearReadRatSlp

Pipe Network motion icon

 Function - Returns the Ratio Slope value of a selected Gear Block from the Pipe Network.

The Ratio Slope sets the limit in 1/Seconds (or s-1) at which step changes in Ratio are implemented.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initialized Gear object.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Slope

LREAL

≥ 0 (zero)

1/sec (or s-1)

  • The Ratio Slope value currently assigned to the selected Gear Pipe Block.
  • This can be a different sign than what is programmed with MLGearWriteRatSlp.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Find the Ratio Slope value of Gear1 Pipe Block
Gear1RatioSlope := MLGearReadRatSlp(PipeNetwork.GEAR1);

See Also