MLMstInit

Pipe Network motion icon

 Function - Initializes a Master TMP generator block.

  • This function is automatically created when the MLMaster Block is included in the Pipe Network Editor.
  • Based on the parameters defined in the Master pipe block, the Inputs for this function are initialized by default.

Figure 1: TMP Initialization

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Master Block.

ModuloPosition

LREAL

No range

User units

No default

Modulo Position for cyclic motion systems expressed in user logical units (Position Rollover Value).

SamplingPeriod

LREAL

No range

Cycles

No default

  • Sampling period of the generator expressed according to the update cycle.
  • Example: 2.0 means the sampling is done once every 2 cycles.

TravelSpeed

LREAL

No range

User units

No default

  • Travel speed value expressed in user position units per second.
  • The travel speed value is used to set the constant speed part of the trapezoidal motion profile (TMP).
  • See Set the Axis Block Position Units.

Acceleration

LREAL

No range

User units / sec2

No default

  • Acceleration value expressed in user position units per second squared.
  • The acceleration value is always used to generate the first part of the trapezoidal motion profile (TMP).
  • See Set the Axis Block Position Units.

Deceleration

LREAL

No range

User units / sec2

No default

  • Deceleration value expressed in user position units per second squared.
  • The deceleration value is always used to generate the last part of the trapezoidal motion profile (TMP).
  • See Set the Axis Block Position Units.

InitialPosition

LREAL

No range

User units

No default

  • Initial position value expressed in user position units.
  • Used only at the pipe activation to initialize the position starting point.

Modulo

BOOL

FALSE, TRUE

N/A

No default

The available modes are:

  • TRUE - Modulo
  • FALSE - No modulo

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Initialize  a Master Pipe Block named "MASTER" to a Modulo of 360, motion generator sample period of 1,Speed of 1000.0, Accel and Decel of 10000.0, Initial position of 0.0,
MLMstInit( PipeNetwork.MASTER, 360.0, 1.0, 1000.0, 10000.0, 10000.0, 0.0, true );