MLMstReadDecel
Function - Gets the present deceleration value of a master block.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
0 to 1 |
N/A |
No default |
Enables the function or function block to be executed. |
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID name of the Master Block. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
|
|
Deceleration |
LREAL |
|
User units / sec2 |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// Read the present deceleration of a Pipe Block named “MASTER”
MLMstReadDecel( PipeNetwork.MASTER );