MLMstWriteDecel

Pipe Network motion icon

 Function - Sets the deceleration of a master block.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

EN

BOOL

FALSE, TRUE

N/A

No default

Enables the function or function block to be executed.

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Master Block.

Deceleration

LREAL

No range

User units / sec2

No default

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MLMstWriteDecel( PipeNetwork.MASTER, 40000.0 );

See Also

MLMstWriteSpeed