MLMstWriteInitPos

Pipe Network motion icon

 Function - Sets the initial position of a master block.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

EN

BOOL

FALSE, TRUE

N/A

No default

Enables the function or function block to be executed.

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Master Block.

Position

LREAL

No range

User units

No default

Initial position.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MLMstWriteInitPos( PipeNetwork.MASTER, 120.0 );