MLPmpReadInitPos
Function - Gets the Initial Position parameter of a PMP block.
- This value is the position the PMP block starts at when the Pipe Network is enabled.
- Can be set when adding a PMP block to a Pipe Network and defining the parameters for that block.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID name of a PMP function block in the Pipe Network. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
InitialPosition |
LREAL |
|
User units |
Present Initial Position of the PMP Pipe Network function block.
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
PmpInitPos := MLPmpReadInitPos( PipeNetwork.PmpMaster ) ;
See Also