MLPhaReadSlope
Function - Gets the phase slope value of a phaser block.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID name of a phaser function block in the Pipe Network. |
Outputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Slope |
LREAL |
|
User units / sec |
Present slope value.
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
PresentSlope :=MLPhaReadSlope( PipeNetwork.PhaseAdjust );
See Also