MLSyncInit

Pipe Network motion icon

 Function - Initializes a synchronizer Pipe Block.

  • Returns TRUE if the function succeeded.
  • This FB is automatically created in the compiled code of a Pipe Network.
  • This function block is part of the MLPN_CREATE_OBJECT to initialize the Pipe Network.
    • It is called at the beginning of an application program with the function call:
PipeNetwork(MLPN_CREATE_OBJECTS);

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Pipe Network Block.

ModuloPosition

LREAL

0 to 1.0x10300

User units

No default

  • Value of the cyclic period of the input signal.
    • Expressed in User units.
  • The parameter is defined to correctly manage the periodicity (modulo) of the input values.
  • 0 (zero) indicates the input signal does not use the modulo operation.

CurveType

DINT

1 to 2

N/A

No default

When synchronizing, specifies which type of curve (parabolic or polynomial) has to be implemented for merging with the master.

The options are:

  • 1 = Parabolic
  • 2 = Polynomial

DeltaS

LREAL

No range

User units

No default

  • The Distance to get in or out of synchronization.
  • This parameter is used in MLSyncStart and MLSyncStop.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Initialize  a synchronizer  Pipe Block named “ SYN” with a modulo of 360, Curve Type of Parabolic, and a distance (DeltaS) of 30 to get in and out of synchronization
MLSyncInit( PipeNetwork.SYN, 360, 1, 30 );

See Also

MLSyncWriteDeltaS