MLTrigIsTrigged

Pipe Network motion icon

 Function - Checks if the selected block has been triggered.

  • When a block has been triggered, it contains the time and position when a Fast Input event occurred.
    • The application has to reset the block before the block can be triggered again.
  • All trigger events that are sent to the block during its triggered state are lost.
  • Once triggered, a block has to be reset before it can be triggered again.
    • All events sent to a block while in a triggered state are ignored.
    • The position and time information is lost.

Fast Homing - Inputs

See these topics:

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initiated Trigger object.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Check if a Trigger Block has been triggered, then save position
IF MLTrigIsTrigged( PipeNetwork.TRIGGER ) THEN
Trig_Position := MLTrigReadPos( PipeNetwork.TRIGGER );
END_IF

See Also