LogFileCSV
Function Block - Create a log file in CSV format for a list of variables.
-
-
- Calling this function can lead to missing several PLC cycles.
- Files are opened and closed directly by the target's Operating System.
- Opening some files may be dangerous for system safety and integrity.
- The number of open files may be limited by the target system.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
LOG |
BOOL |
FALSE, TRUE |
N/A |
No default |
Variables are saved on any rising edge of this input. |
|
RST |
BOOL |
FALSE, TRUE |
N/A |
No default |
Reset the contents of the CSV file. |
|
LIST |
DINT |
No range |
N/A |
No default |
ID of the list of variables to log (use VLID function). |
|
PATH |
STRING |
1 to 255 |
N/A |
No default |
Path name of the CSV file.
|
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
N/A |
TRUE if the requested operation has been performed without error. |
|
ERR |
DINT |
No range |
N/A |
Error report for the last requested operation. 0 (zero) is OK. |
Remarks
- By default, the LogFileCsv block uses:
- Semicolons ( ; ) as field separators.
- Dots ( . ) as decimal points.
- The SetCsvOpt function to modify these characters to suit specific formatting requirements.
- Opening a file may be unsuccessful (e.g., invalid path or file name, too many open files, etc.)
Your application has to process such error cases in a safe way. - Valid paths for storing files depend on the controller and the type of file storage media being used.
- See:
- File Path Conventions
- SD Card Path Conventions
- Shared Directory Path Conventions
- USB Flash Drive Path Conventions
- See:
- This function enables to log values of a list of variables in a CSV file.
- On each rising edge of the LOG input, one more line of values is added to the file.
- There is one column for each variable, as they are defined in the list.
- The list of variables is prepared using a text editor.
- Use the VLID function to get the identifier of the list.
- On a rising edge of the RST command, the file is emptied.
- When a LOG or RST command is requested, the Q output is set to TRUE if successful.
- In case of error, a report is given in the ERR output.
- Possible error values are:
- 1 = Cannot reset file on a RST command.
- 2 = Cannot open file for data storing on a LOG command.
- 3 = Embedded lists are not supported by the runtime.
- 4 = Invalid list ID.
- 5 = Error while writing to file.
- Possible error values are:
- Combined with real time clock management functions, this block provides a very easy way to generate a periodical log file.
Figure 1 (
) shows a list and a program that log values every day at 14h23m (2:23 pm).
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MyLOG is a declared instance of LogFileCSV function block *)
MyLOG (b_LOG, RST, LIST, PATH);
Q := MyLOG.Q;
ERR := MyLog.ERR;
See Also