SetWithin

.PLCopen motion icon

 Function - Force a value when inside an interval.

  • The output is forced to VAL when the IN value is within the [MIN ... MAX] interval.
  • It is set to IN when outside the interval.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN

ANY

 

 

 

Input.

MIN

ANY

 

 

 

Low limit of the interval.

MAX

ANY

 

 

 

High limit of the interval.

VAL

ANY

 

 

 

Value to apply when inside the interval.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

ANY

 

 

Result.

Truth Table

In

Q

IN < MIN

IN

IN > MAX

IN

MIN < IN < MAX

VAL

FBD Language Example

Not available.

FFLD Language Example

Not available.

IL Language Example

Not available.

ST Language Example

Not available.