Subtraction -

Operator - Performs a subtraction of all inputs.

  • All inputs and the output must have the same type.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN1

ANY_NUM / TIME

 

 

 

First input.

IN2

ANY_NUM / TIME

 

 

 

Second input.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

ANY_NUM / TIME

 

 

Result: IN1 - IN2.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung (ENO) keeps the same value as the input rung.
    • The subtraction is executed only if EN is TRUE.
    • ENO is equal to EN.

IL Language Example

Not available.

ST Language Example

Q := IN1 - IN2;

See Also