max

PLCopen motion icon

 Function - Get the maximum of two integers.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN1

ANY

 

 

 

First input.

IN2

ANY

 

 

 

Second input.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

ANY

 

 

IN1 if IN1 > IN2; IN2 otherwise.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung keeps the state of the input rung.
    • The comparison is executed only if EN is TRUE.
    • ENO has the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := MAX (IN1, IN2);

See Also