Assignment :=
- The output variable and the input expression must have the same type.
- The forced variable cannot have the read-only attribute.
- In the FBD and FFLD languages, the 1 block is available to perform a 1 gain data copy (1 copy).
- In the IL Language:
- The FFLD instruction loads the first operand.
- The ST instruction stores the current result into a variable.
- The current result and the operand of ST must have the same type.
- Both FFLD and ST instructions can be modified by N in case of a Boolean operand for performing a Boolean negation.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
ANY |
|
|
|
Any variable or complex expression. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
ANY |
|
|
Forced variable. |
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the assignment.
- The output rung keeps the state of the input rung.
- The copy is executed only if EN is TRUE.
- ENO has the same value as EN.
IL Language Example
Not available.
ST Language Example
Q := IN; (* copy IN into variable Q *)
Q := (IN1 + (IN2 / IN 3)) * IN4; (* assign the result of a complex expression *)
result := SIN (angle); (* assign a variable with the result of a function *)
time := MyTon.ET; (* assign a variable with an output parameter of a function block *)
See Also