WHILE DO END_WHILE
Syntax
WHILE <BOOL expression> DO
<statements>
END_WHILE;
Remarks
- The statements between DO and END_WHILE are executed while the Boolean expression is TRUE.
- The condition is evaluated before the statements are executed.
- If the condition is FALSE when WHILE is first reached, statements are never executed.
-
-
- Loop instructions can lead to infinite loops that block the target cycle.
- Never test the state of an input in the condition because the input is not refreshed before the next cycle.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
iMax := 10;
WHILE iPos < iMax DO
MyArray[iPos]:=0;
iPos +:=1;
END_WHILE;
See Also