S
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
SET |
BOOL |
FALSE, TRUE |
|
|
Condition. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
|
Output to be forced. |
Truth Table
|
SET |
Q prev |
Q |
|---|---|---|
|
0 |
0 |
0 |
|
0 |
1 |
1 |
|
1 |
0 |
1 |
|
1 |
1 |
1 |
FBD Language Example
- In the FBD Language, RS and SR function blocks are preferred.
FFLD Language Example
- In the FFLD Language, they are represented by (S) and (R) coils.
Example: Use of S coil:
IL Language Example
Not available.
ST Language Example
Not available.
See Also