DTGetNTPServer
Function Block - Read the NTP server address.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, request to read the NTP server address. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
No range |
N/A |
Indicates the error if Error output is TRUE. Error Codes
|
|
NTP Server |
STRING |
No range |
N/A |
The address of the NTP server used for clock synchronization. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// read the NTP server address
Inst_DTGetNTPServer( bGetNTPServer );
if Inst_DTGetNTPServer.Done then
bGetNTPServer := false;
if NOT Inst_DTGetNTPServer.Error then
NTPServer := Inst_DTGetNTPServer.NTPServer;
else
ErrorID := Inst_DTGetNTPServer.ErrorID;
end_if;
end_if;
See Also