DTSetTimeZone
Function Block - Set the time zone.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Execute |
BOOL |
FALSE, TRUE |
N/A |
No default |
If TRUE, request to set the time zone. |
|
TimeZone |
STRING |
No range |
N/A |
No default |
The time zone the controller should use. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the command completed successfully. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
DINT |
No range |
N/A |
Indicates the error if Error output is TRUE. Error Codes
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// configure the time zone
Inst_DTSetTimeZone( bSetDTZone, TimeZone );
if Inst_DTSetTimeZone.Done then
bSetDTZone := false;
bError := Inst_DTSetTimeZone.Error;
ErrorID := Inst_DTSetTimeZone.ErrorID;
end_if;
See Also