LDT_Now
Function - Reports the current system time as a long date and time (LDT).
- The returned value is time-zone independent.
- Use LDT_To_DTL_Local or LDT_To_DTL_UTC to convert it to a calendar date and time.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
output |
LDT |
N/A |
N/A |
No default |
A variable where the present system time is written. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
N/A |
If TRUE, the present time was read successfully. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
// Obtain the current time, then convert it to a local calendar date and time.
Ok := LDT_Now(MyLDT);
IF Ok THEN
Ok := LDT_To_DTL_Local(MyLDT, MyDTL);
IF Ok THEN
// MyDTL now holds the current local calendar date and time.
END_IF;
END_IF;