LT <

PLCopen motion icon

Operator - Test if the first input is less than the second input.

  • Both inputs must have the same type.
  • Comparisons can be used with strings.
    • With strings, the lexical order is used for comparing the input strings.
      • Examples:
        ABC is less than ZX.
        ABCD is greater than ABC.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN1

ANY

 

 

 

First input.

IN2

ANY

 

 

 

Second input.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

BOOL

 

 

TRUE if IN1 < IN2.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung is the result of the comparison.
  • The comparison is executed only if EN is TRUE.

IL Language Example

Not available.

ST Language Example

Q := IN1 < IN2;

See Also