num_to_string

PLCopen motion icon

 Function - Converts a number into a string value.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN

ANY

 

 

 

Input number.

Width

DINT

 

 

 

Length of the output string.

Digits

DINT

 

 

 

Number of digits after decimal point.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

STRING

 

 

Value converted to string.

Remarks

This function converts any numerical value to a string.

It allows a specific length and a number of digits after the decimal points.

WIDTH

If WIDTH is 0 (zero), the string is formatted with the necessary length.

Q := NUM_TO_STRING (1.333333, 0, 2);    (* Q is '1.33' *)

If WIDTH is greater than 0 (zero), the string is completed with leading blank characters to match the value of WIDTH.

Q := NUM_TO_STRING (123.4, 8, 2);    (* Q is '   123.40' *)

If WIDTH is greater than 0 (zero), the string is completed with trailing blank characters to match the value of WIDTH.

Q := NUM_TO_STRING (123.4, -8, 2);    (* Q is '123.40  ' *)

DIGITS

If DIGITS is 0 (zero), neither decimal part nor decimal point are added.

Q := NUM_TO_STRING (1.333333, 3, 0);    (* Q is '   1' *)

If DIGITS is greater than 0 (zero):

  • The corresponding number of decimal digits are added.
  • '0' digits are added if necessary.
Q := NUM_TO_STRING (1.333333, 0, 1);    (* Q is '1.3' *)

If the value is too long for the specified width, the string is filled with '*' characters.

Q := NUM_TO_STRING (1234, 3, 0);    (* Q is '***' *)

FBD Language Example

Not available.

FFLD Language Example

Not available.

IL Language Example

Not available.

ST Language Example

Not available.