CTU / CTUr

PLCopen motion icon

 Function Block - Up counter.

  • The counter is empty (CV = 0) when the application starts.
  • The counter does not include a pulse detection for CU input.
  • Use the f_trig or r_trig function blocks for counting pulses of CU input signal.
  • CTDr, CTUr, and CTUDr function blocks operate exactly as other counters.
    • Exception: All Boolean inputs (CU, CD, RESET, LOAD) have an implicit rising edge detection included.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

CU

BOOL

 

 

 

  • Enable counting.
  • Counter is increased on each call when CU is TRUE.

PV

DINT

 

 

 

Programmed maximum value.

RESET

BOOL

 

 

 

  • Reset command.
  • Counter is reset to 0 when called with RESET to TRUE.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

CV

DINT

 

 

Current value of the counter.

Q

BOOL

 

 

TRUE when counter is full (i.e., when CV = PV).

FBD Language Example

FFLD Language Example

  • In the FFLD Language, CU is the input rung.
    • The output rung is the Q output.

IL Language Example

Not available.

ST Language Example

(* MyCounter is a declared instance of CTU function block. *)
MyCounter (CU, RESET, PV);
Q := MyCounter.Q;
CV := MyCounter.CV;

See Also