EnableEvents

PLCopen motion icon

 Function - Enable or disable the production of events for binding (runtime to runtime variable exchange).

  • Production is enabled when the application starts.
  • The first production is operated after the first cycle.
  • To disable events since the beginning, you must call EnableEvents (FALSE) in the very first cycle.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

EN

BOOL

FALSE, TRUE

 

 

  • TRUE to enable events.
  • FALSE to disable events.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

ENO

BOOL

FALSE, TRUE

 

Echo of EN input.

FBD Language Example

FFLD Language Example

  • The input rung (EN) enables the event production.
    • The output rung keeps the state of the input rung.
    • Events are enables if EN is TRUE.
    • ENO has the same value as EN.

IL Language Example

Not available.

ST Language Example

ENO := EnableEvents (EN);

See Also

Alarm_A