FatalStop
Function - Breaks the cycle and stop with fatal error.
- This function breaks the current cycle and sets the Virtual Machine in ERROR
mode.
- Restarting normal execution is performed using the debugger.
- The VM is stopped only if the IN argument is TRUE.
- The end of the current cycle is then not performed.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
BOOL |
FALSE, TRUE |
|
|
Condition. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
BOOL |
FALSE, TRUE |
|
TRUE if performed. |
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
Not available.
See Also