ror
Function - Rotate bits of a register to the right.
Arguments can be signed or unsigned integers from 8- to 32-bits.
Diagram
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
ANY |
|
|
|
Register. |
|
NBR |
ANY |
|
|
|
Number of rotations (each rotation is 1 bit). |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
ANY |
|
|
Rotated register. |
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the operation.
- The output rung keeps the state of the input rung.
- The rotation is executed only if EN is TRUE.
- ENO keeps the same value as EN.
IL Language Example
Not available.
ST Language Example
Q := ROR (IN, NBR);
See Also