concat

PLCopen motion icon

 Function - Concatenate of strings.

  • In the FBD Language or FFLD Language, the block can have up to 16 inputs.
  • In the IL Language or ST Language, the function accepts a variable number of inputs (at least 2).
  • Use the + operator to concatenate strings.

Inputs

Input

Data Type

See Data Types.

Range

Unit

Default

Description

IN_1

STRING

 

 

 

Any string variable or constant expression.

IN_N

STRING

 

 

 

Any string variable or constant expression.

Outputs

Output

Data Type

See Data Types.

Range

Unit

Description

Q

STRING

 

 

Concatenation of all inputs.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Q := CONCAT ('AB', 'CD', 'E');
(* now Q is 'ABCDE' *)