udpSendToArray
Function - Sends a byte array through UDP.
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0 to 1 |
N/A |
No default |
Execute the function. |
|
sock |
DINT |
0 to 65535 |
N/A |
No default |
Socket number, return value from udpCreate. |
|
nb |
DINT |
0 to 65535 |
N/A |
No default |
Number of bytes to be transferred. |
|
add[ ] |
USINT |
0 to 32 |
N/A |
No default |
Array which contains information about the server. |
|
data[ ] |
USINT |
0 to 65535 |
N/A |
No default |
Array of bytes to be transferred. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
|
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Success:= udpSendToArray(Socket_Number,nb,add,Frame);