NVRAM
KAS uses NVRAM to save Retain Variables.
|
Hardware Type |
NVRAM Size Allocation |
|---|---|
|
KAS Simulator |
256 Kbytes |
|
PCMM2G |
256 Kbytes |
-
-
Part of NVRAM allocation is reserved to store some internal data (144 bytes).
As a consequence, not all of the complete physical NVRAM is available for the retain variables.
If the size is big enough, KAS updates the non-volatile memory to store the retain variables values.
- This operation is performed in the background every 20 seconds.
- The frequency increases to every two seconds when the application is running or when you shutdown the application.
NVRAM Life Expectancy
- Data Retention: At maximum operating temperature, the data written to the memory is retained for 10 years.
- Endurance: NVRAM memory has an endurance limit of 1014 read / write accesses.
- More than 6,000,000 years of being accessed every 2 seconds.
-
-
- Using the retain variables is very cycle time consuming.
- As a consequence, Kollmorgen strongly recommends to carefully monitor the system load with the TraceTimes command.
- See Oscilloscope Control Panel.
Verify the NVRAM Space
To calculate NVRAM space, add the size of each retained variable according to the:
- Data Types
- Arrays - The numbers of elements in case the variable is declared as an array.
Remember! Add the 144 bytes!
In Figure 1, the total size is: 3684 bits (which is less than 0.5 Kbytes).
Figure 1: Example: Retain variables
|
Variable |
Size / element |
Number of Element |
Total Size / variable |
|---|---|---|---|
|
bLedStatus |
1-bit |
4 |
4 |
|
Internal data |
1152-bits (144 bytes) |
N/A |
1152 |
|
MasterAbsPos |
64-bits |
1 |
64 |
|
MyString |
800-bits (100 bytes) |
3 |
2400 |
|
TravelSpeed |
64-bits |
1 |
64 |