EtherCAT: ERROR: Failed to retrieve Vendor…
or
EtherCAT: ERROR: Failed to retrieve EtherCAT device…
These errors indicate either:
- The ESI file for the EtherCAT device is missing.
- Information is missing from the ESI file for a device and/or module.
Examples
EtherCAT: ------------- Generating EtherCAT Network Information (ENI) file ---------------
EtherCAT: ERROR: Failed to retrieve Vendor for vendorID=0x21 in ESI cache
Project compile failed
EtherCAT: ------------- Generating EtherCAT Network Information (ENI) file ---------------
EtherCAT: ERROR: Failed to retrieve EtherCAT device (vendorID=0x2, productCode=0x44c2c52, revision=0x120000) in ESI cache
Project compile failed
Error Correction
- Identify which EtherCAT devices or modules are listed as Unknown in the Project View.
- Import an appropriate ESI file.
See Also